This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Booting MonvistaLinux on DM6446

Hello everybody

My boot kernel is LSP 02.00.00.140(kernel 2.6.18) and my target file system is MV Pro. 5.0 target file system

When booting kernel , my booting message is stall at " Free init memory :164K "  ,there is my booting message:


Booting PSP Boot Loader

Starting NAND Copy

Booting Application @ 0x81080000


U-Boot 1.2.0 (Jan 31 2008 - 15:59:12)

I2C:   ready
DRAM:  256 MB
unknown vendor=0 Flash:  0 kB
NAND:  64 MiB
In:    serial
Out:   serial
Err:   serial
ARM Clock :- 297MHz
DDR Clock :- 162MHz
MSP430 Firmware supports AM/PM Feature
Hit any key to stop autoboot:  0
TFTP from server 192.168.0.2; our IP address is 192.168.0.3
Filename 'uImage'.
Load address: 0x80700000
Loading: #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         ###########
done
Bytes transferred = 1720056 (1a3ef8 hex)
## Booting image at 80700000 ...
   Image Name:   Linux-2.6.18_pro500-davinci_evm-
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1719992 Bytes =  1.6 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
OK

Starting kernel ...

Uncompressing Linux.............................................................
................................................... done, booting the kernel.
Linux version 2.6.18_pro500-davinci_evm-arm_v5t_le (root@localhost.localdomain)
(gcc  4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 Fri Oct 30 23:37:4
4 CST 2009
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci DM6443 variant 0x0
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists.  Total pages: 30208
Kernel command line: console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nf
sroot=192.168.0.2:/home/blackdan/workdir/filesys,nolock mem=118M
PID hash table entries: 512 (order: 9, 2048 bytes)
Clock event device timer0_0 configured with caps set: 03
Console: colour dummy device 80x30
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 118MB = 118MB total
Memory: 115840KB available (2749K code, 846K data, 164K init)
Security Framework v1.0.0 initialized
SELinux:  Initializing.
SELinux:  Starting in permissive mode
selinux_register_security:  Registering secondary module capability
Capability LSM initialized as secondary
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
NET: Registered protocol family 16
DaVinci: 71 gpio irqs
Generic PHY: Registered new driver
usbcore: registered new driver usbfs
usbcore: registered new driver hub
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 4096 bind 2048)
TCP reno registered
davinci_spi_board_init: NO spi support
Enabling VLYNQ clock
MUX: initialized VLINQEN
MUX: initialized VLINQWD
audit: initializing netlink socket (disabled)
audit(0.350:1): initialized
VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
Installing knfsd (copyright (C) 1996 okir@monad.swb.de).
SELinux:  Registering netfilter hooks
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered
io scheduler deadline registered
io scheduler cfq registered (default)
Non-volatile memory driver v1.2
Serial: 8250/16550 driver $Revision: 1.90 $ 4 ports, IRQ sharing enabled
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfec20000 (irq = 40) is a 16550A
RAMDISK driver initialized: 16 RAM disks of 16384K size 4096 blocksize
Broadcom BCM5411: Registered new driver
Broadcom BCM5421: Registered new driver
Broadcom BCM5461: Registered new driver
Broadcom BCM5481: Registered new driver
DaVinci EMAC: Unable to read MAC from EEPROM, no i2c support in kernel.
TI DaVinci EMAC: MAC address is deadbeaf
TI DaVinci EMAC Linux version updated 4.0
TI DaVinci EMAC: Installed 1 instances.
i2c /dev entries driver
Uniform Multi-Platform E-IDE driver Revision: 7.00alpha2
ide: Assuming 50MHz system bus speed for PIO modes; override with idebus=xx
ide-floppy driver 0.99.newide
usbcore: registered new driver libusual
usbcore: registered new driver hiddev
usbcore: registered new driver usbhid
drivers/usb/input/hid-core.c: v2.6:USB HID core driver
mice: PS/2 mouse device common for all mice
md: md driver 0.90.3 MAX_MD_DEVS=256, MD_SB_DISKS=27
md: bitmap version 4.39
TCP bic registered
Initializing XFRM netlink socket
NET: Registered protocol family 1
NET: Registered protocol family 17
Time: timer0_1 clocksource has been installed.
Sending DHCP requests .., OK
IP-Config: Got DHCP answer from 192.168.0.1, my address is 192.168.0.103
IP-Config: Complete:
      device=eth0, addr=192.168.0.103, mask=255.255.255.0, gw=192.168.0.1,
     host=192.168.0.103, domain=, nis-domain=(none),
     bootserver=192.168.0.1, rootserver=192.168.0.2, rootpath=
md: Autodetecting RAID arrays.
md: autorun ...
md: ... autorun DONE.
Looking up port of RPC 100003/2 on 192.168.0.2
Looking up port of RPC 100005/1 on 192.168.0.2
VFS: Mounted root (nfs filesystem).
Freeing init memory: 164K

 

How could I solve this problem?

Best Regard

Dan