Part Number: AM5728
Tool/software: Linux
Hi Biser,
I am working on TMDSEVM572X development boards from TI.
I have mSATA III SSD from ATP (log from my host machine [ 0.704943] ata4.00: ATA-9: ATP SATA III mSATA, N0516B, max UDMA/133)
I went trough the previous post for mSATA SSD on AM5728 based EVM, I understood it does not support backward compatibility to SATA Gen III devices due to hardware bug. Does the issue still persists ??
Following is the boot log on EVM, when mSATA SSD is connected
[ 9.928640] scsi host0: ahci
[ 9.953268] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a1410ff] port 0x100 irq 348
[ 9.985169] [drm] Initialized pvr 1.14.3699939 20110701 on minor 1
[ 10.011274] vip 48990000.vip: loading firmware vpdma-1b8.bin
[ 10.028661] vip 48990000.vip: VPDMA firmware loaded
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started Telephony service.
[ 10.328679] ata1: SATA link down (SStatus 0 SControl 300)
Out of your experience, please suggest suitable mSATA SSD for the EVM with read speeds upto 300MBps.
Thanks & Regards,
Vamshi G.