Other Parts Discussed in Thread: TMS320C6748
Hi,
We are using TMS320C748 processor which will be connectd to FPGA .We have to use UPP for data transfer between FPGA and processor bidirectionaaly using single channel . One channel(Channel A) i will be using as Transmitter which will be connected to other processor .The other channel (Chan B) will be connected to FPGA as bidirectional. That is it should receive data from FPGA for some duration say 2.5ms and then it should send the processed data to the FPGA on the same channel.
My question is is it possible to configure single channel as both transmitter and Reciever when other channel is always in transmitter whcih will be connected to other processor.
I need to do this without using DSP BIOS .Please send me if any UPP sample code without DSP BIOS. Please help in this regard.
Thanks
Sathya