This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2EVM5777: Infoadas build error

Part Number: TDA2EVM5777

Hi,

While trying to setup Infoadas package, its asks to run  ./build.sh --all install as a prerequisite. While doing this i got a libdrm_omap error. How to fix this?


checking for DRM... no
configure: error: Package requirements (libdrm libdrm_omap) were not met:

No package 'libdrm_omap' found

Consider adjusting the PKG_CONFIG_PATH environment variable if you
installed software in a non-standard prefix.

Alternatively, you may set the environment variables DRM_CFLAGS
and DRM_LIBS to avoid the need to call pkg-config.
See the pkg-config man page for more details.

Some other questions i have is 

while running this command
sudo ./mk-sd-update.sh <path to infoadas prebuilt folder> [path to targetfs] [path to boot patition]
What is the targetfs path is it the targetfs downloaded for Processor SDK compilation
Which boot partion i need to give? Is it the boot folder in ti-infoadas_dra7xx-evm_2_00_00_01/prebuilt/boot
Which path i should give for VISIONSDK_FW_PATH? is it ti-infoadas_dra7xx-evm_2_00_00_01/visionsdk-fw