This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5728: DMM peg priority for IVA-HD

Part Number: AM5728

Tool/software: Linux

Hi.

I readed DMM peg priority for IVA-HD and now i don't understand it as below it.

devmem2 0x4E000624 w 0x48444444

it is shown at TRM document as below it.

14.2.3.2.3 Mater NIU Identification

        Table 14-10. ConnID Values

8-bit ConnID(hex)        4-bit ConnId(hex)       Master NIU

3A                                       3                             IVA

so, ConnID value of IVA is 3 not E.

and i don't find DMM_PEG_PRIO_k(1) is IVA.

Is right as  devmem2 0x4E000624 w 0x48444444  for highest priority of IVA  ?

Thanks a lot.