This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/DRA726: Issues with delay for application load with weston

Part Number: DRA726


Tool/software: Linux

Our customer application uses embedded wizard. I set it as a client in weston.ini

The problem is that it takes about 10 seconds for the application to appear on the screen. Is there a better way to load the application than setting it as a client?

If I just power up with the weston desktop it doesn't have that long delay and loading the application using ssh gets the program to load right away.

Michel Catudal

ACTIA Corp