This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Starterware/TDA3: Input interrupt test application for GPIO on Starterware doesn't work properly

Part Number: TDA3


Tool/software: Starterware

I have a problem with Input interrupt test application for GPIO.

It's based on interrupts and I need to provoke hardware interrupt (to connect  GPIO pin that I'm testing with a ground) to get corresponding output in the console. My GPIO pin is on J28 connector and I tried to connect it to the ground directly - using wire, after I loaded app on M4 core using Code Composer Studio. It doesn't work and my Code Composer Studio crashes down with 'power loss' message in the same moment when I connect those two dots on the board with a wire.

I think that I am not supposed to that from hardware point of view, so my question is: does anyone know any smarter way of testing this app on TDA3x board?

Best regards,

Jho.