This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM4378: Error in QT based "CAN" application

Part Number: AM4378


Tool/software: Linux

Dear Sir,

I have developed a board based on AM4378 and developing a QT based "CAN" (serial bus based application) which resides under example/serial bus/can.

While building a application, it throws below error.

"Project ERROR:Unknown module() in QT : serial bus "

How do i solve this issue?

My development details are as given below.

IDE : QT Creator

target operating system : sitara linux

Host operating system : Linux.

Regards,

Winiston.P