Other Parts Discussed in Thread: AM5728
Hi,
I bought a TI AM5728 EVM (TMDSEVM572X) and the module camera both the 4/24/2017.
From the beginning, when I used the main board and pluged the camera on it, we found some problem : sometimes the camera is recognize by the system and sometimes it"s not recognize.
We have updated the software as requested by the support : we had update the linux to the last stable 4.10.17 version and update Gstreamer 1.0 verion 1.10.x
So the camera still work at part time.
When the the camera is work and unfortunatly when we touch lightly the camera, then it will stop working and the system freeze. We have to reboot the system.
It's seems the problem come from the connector.
How can I do to resolv the issue ?
Is it possible to change the items ?
We can not work on our project with, so I bought an another item the 5/29/2017.
Thank to Help us.