Other Parts Discussed in Thread: TPS65217
Tool/software: Linux
To whom it may concern,
We're using a custom board based on the BeagleBone Black, and are experiencing a "System time loop" similar to those in these threads:
https://e2e.ti.com/support/arm/sitara_arm/f/791/p/506562/1837427
Proc: AM3352B ZCZ A100
Clocks: 24MHz, 32.762kHz crystals are installed, OSC[1:0] grounds are tied to board ground (advisory 1.0.30)
Maxim i2c RTC chip used to for linux RTC function
Power: TPS65217 replaced with TP65910
The issue appears after several hours to several days of continuous operation.
We've been using this board design for almost a year without this issue appearing,
So far we've detected the issue in our most recent run (date/lot code 63ARZCW) although it may exist on older runs as well.
Are there any known fixes?
Thanks for your help,
Kyle