This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DVSDK for DSP-only DaVinci processors (6437)?

Does TI have a DVSDK available for DSP-only DaVinci processors, specifically the DM6437? I have looked, but I couldn't find one (at least not in similar locations as the linux DVSDKs and/or WinCE versions for other processors).

I see VPFE/VPBE, pin multiplexing, etc application notes on the product page which contain drivers and example code, but is there a compilation that aggregates everything as a whole?

Thanks!

Derek

  • Derek Walters said:
    Does TI have a DVSDK available for DSP-only DaVinci processors, specifically the DM6437?

    Yes, however it has not been relicensed to be made available through a publicly accessible link, at least not without logging into my.ti and registering a board. This being said, you can access the download site by registering a DM6437 EVM board through www.ti.com/davinciregistration much like you had to do in the olde days for other Davinci boards before the download links were made public.

    Derek Walters said:
    I see VPFE/VPBE, pin multiplexing, etc application notes on the product page which contain drivers and example code, but is there a compilation that aggregates everything as a whole?

    The DVSDK for DM6437 includes the PSP and demo software, though not all the application notes are necessarily included, it is still what I would recommend to get started as a software package for the DM6437.