This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Developing Embedded Software using DaVinci and OMAP Technology book

I have been working through the book above and it references an example using the DM355 (IPNetCam Refernece design) which is in the SDK for that device.  I have set up with my DM365 toolchain, examples, etc but have no source/ipnc_app_ .... to copy. 

There is no file on the web so can you please point me where I can just get these source files from (without needed to intstall a full sdk for the device).

 

  • Though I am not very familiar with this book, I can say that the IP Net Cam reference designs (of which there are both DM355 and DM365 versions available here) have seperate software on top of the typical DVSDK software release, and to access that software you may actually have to purchase the particular IP net cam design. You may want to contact the author of the book to get some clarification as to which particular kit was used if it is not obvious from the book.

  • Thanks for the reply, I will contact the book people (Morgan & Claypool Publishers) but I originally posted in here as I thought TI was more involved in it (Foreward is by Gene A Frantz - Principal Fellow, Texas Instruments Inc.).