Part Number: TDA2EG
Tool/software: TI C/C++ Compiler
HI,
We are using TDA2xx board along with “VisionSDK” application board.
We are using it for our “Single camera application Use cases” and development purpose for the same.
Downloading the image file:
We are downloading the image files to the board either using CCS/ SD card.
Current Issue:
We are able to download the image and in Hyper Terminal, we are getting the Use-case Menu.
When selecting the “Single Camera Use case” and trying to run the simple “Capture and Display” Use case, the video frames are NOT getting displayed on the screen.
It is only showing the “Core Usage” information in the display, but the image frames are NOT there.
Sometimes we got the display, after that it is not working with Camera Use cases.
We are not getting any errors when executing the use case.
- We also tried changing the camera, still it is not working.
- We tried to run the “Network use case”. That is displaying properly. So the TDA2xx board has no issues, the application board is having the problem.
We have attached the screen shot of the display.
Kindly suggest the procedures for resolving this issue.