Other Parts Discussed in Thread: THS7303, PCA9543A
Tool/software: Linux
I have a DM368EVM MISTRAL board. Im trying to boot it from SD card from the box. Kernel log is
ths7303 1-002c: chip found @ 0x58 (DaVinci I2C adapter)
vpfe_init
vpfe-capture: vpss clock vpss_master enabled
vpfe-capture vpfe-capture: v4l2 device registered
vpfe-capture vpfe-capture: video device registered
dm365evm_enable_pca9543a
dm365evm_enable_pca9543a, status = -121
EVM: switch to HD imager video input
mt9p031 1-005d: No MT9P031 chip detected, register read ffffff87
vpfe-capture vpfe-capture: v4l2 sub device mt9p031 register fails
No sub devices registered
vpfe-capture: vpfe capture clocks disabled
vpfe_register_ccdc_device: DM365 ISIF
dm365_isif: probe of dm365_isif failed with error -22
I can not stand how to capture video ftom cvbs input.
When I make my own SD card form BSP, I see the same kernel log, and I dont see /dev/video0 device
Why board from the box doesn't work, and how to make it work?
I tried BSP 4.0.2 and 4.0.1 for DM368 EVM.