I have a need to do a demonstration of two simultaneous video compressions with 1 frame latency. The input comes from two HDMI, 720P video streams. I plan to use two TVP7002 to capture the HDMI signals and send the digital video to the DM648 video in ports. My questions are:
- Does the DM648 come with the video compression demo that I can modify to use only I-frame? Do you have JPEG2000 CODEC for DM648?
- Can the DM648 compress two 720P video streams in one frame time?
If the answers above are no; especially it it needs two DM648 for compressing the 2 video streams, then when should I pick the DM6467 vs. the DM648? Would it be better to use two DM6467? Would the DM6467 have more samples, demo codes, and technical support than the DM648 that I can leverage?
Regards,
Sy