This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6657 PCIE link speed problem

Hi Volks,

I am using C6657 DSP on our custom board and using CCSV7.1. I am testing the throughput of PCIE interface between DSP and FPGA. As the reference clock is 100MHz.i am using the default value 0x1c9(PLLM - 64h) for PCIE_SERDES_CFGPLL.

At the beginning when i use the PCI operationg mode, Gen 1 i am expecting 2.5 GHz PLL output, but getting only 1.2 GHz.  when i changed the PCI operating mode Gen1 to Gen2, and i am expecting 5GHz PLL output getting only 2.5 GHz. 

do any one have any idea, what can be the reason?

Thanks,

Ram.