Other Parts Discussed in Thread: OMAP3530
I’ve got a question, What if the sys_nrespwron pin comes up with the vdds and vdds_mem and is stable at 1.8 volts for about 200us. See attached omap3530_CUS_power_up_sequence.bmp. It is then held low until VDD_core is brought up and then toggled. Would this cause the system to be locked in a kind of reset state?
The TEK0003 shows the same pins but is after a quick power cycle. How do I add attachments.? thanks..