hello:
we are using a DM6467T evm board to switch from nand to pci, we select the pci bus support in kerenl, and boot from tftp,
when the kernel is uncompressed and runs to switch from nand to pci, the DM6467T evm board resets.
1) we use TMS320DM6467 HD 1080P Evaluation Module , DM6467T(1Ghz) , and the board is not plugging in pci slot.
2) SW3 set :1110 0000,select " NAND Flash boot";
3) after Uboot finished,we use tftp download uImage
4) uImage unzip, run ... when run to "nand flash -> PCI"("davinci_cfg_reg(DM646X_PCIEN)" ),reset again。
(1) Uboot
2) download uImage ,unzip
3)unzip, ...... reset
4)we use:2.6.32-rc2,and select " PCI "