Part Number: TMS320C6657
Hi,
I have questions about C6657.
Q1.
C6657 L1P cache are supporting Error Detection but it's not supporting Error Correction.
So, my customer want to know the soft error rate of L1P.
Is there any data of L1P soft error rate?
Q2.
If L1P soft error occured, is it possible to detect the address where the error occured
and is it possible to read from the real address?
Q3.
When the error interrupt will occur?
Is it just after reading the address where the error occur?
Or, will the error interrupt occur after executing the next instruction?
Q4.
If L1P soft error occured, will the cache be invalidated automatically then re-read from the real address
and the instruction which error occured will be executed again?
best regards,
g.f.