Tool/software: Linux
Hello,
I am referring to the following page:

1. However, PSP 04.07.00.02 Supports 2.6.37. I wanted to check if TI814X is supported in newer kernels Such as 3.xx or 4.xx Kernels.
2. Also, Which PSP is the latest and recommended. We are looking for PCI support and Video Input Support.
3. On the Video Input Port Support - Do i need the HDVPSS packge or the drivers are present in Linux OS itself.
Thanks