Other Parts Discussed in Thread: UCD9244
Hi
After following the getting started guide, the module reports a SoC Power failure. The BMC version is 1.0.2.6. Can someone assist me in getting this resolved.
Larry
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
After following the getting started guide, the module reports a SoC Power failure. The BMC version is 1.0.2.6. Can someone assist me in getting this resolved.
Larry
Hello Rahul,
The first link to the known issues for a 4.0 rev of the EVM the Adavntech states the following:
A revised UCD configuration has been created to eliminate this VDD33 supply
instability. The digital control loop compensation was changed to put Fz1 at half of
the double pole frequency and Fz2 at the double pole frequency. Then the gain was
reduced to limit the bandwidth to 5% of the switching frequency. This new UCD9244
XML File configuration is named UCD9244_52_A05.XML. It can be loaded directly in
to the UCD9244 controller using the TI tool Fusion Digital Power Designer. A script is
also available to perform a field update through the serial port using the BMC. This
script file is named UCD9244_52_A05.txt. These files are available on this website.
Please follow the instructions at
processors.wiki.ti.com/.../EVMK2H_Hardware_Setup
anagement_Field_Update) to perform this field update.
Following thread there is no discussion on the Rev 4 version of this board.
It appears that I'm being asked to fix a problem that should not see. Can I get an RMA and shipping account information to return this board? I would like to exchange this for a known working board.
Larry
Larry,
We understand that this is causing difficulty for you. Unfortunately, RMA replacement for this issue is not the solution. It will cause much more trouble and delay that simply loading the new configuration files. Be sure that you use both the latest configuration files and the updated bmc_tool.py tool. The E2E link below is an example of a user that was able to get their platform working as intended.
Larry,
We have updated the instructions and made sure that they point to the correct versions of the files on the EVM manufacturer's web page. (The EVM manufacturer's web page has tabs for older versions of the EVM and these other tabs contain out-of-date files.) This information is all linked from:
Use of the proper version of the bmc_tool.py script with the latest versions of the UCD configuration files will result in a functional K2H EVM.
Tom