I would like to use the PRTCSS to control the DM365's 3.3V then 1.8V then 1.35V power off sequence, but have some questions:
According to SPRUFJ0A, Section 3.4, the power off sequence provides two output signals, PWCTRO0 and PWCTRO1, that control RESET and Power Down. Is this hard-coded, or if it is simply a recommended configuration? I need at least 3 output signals to perform the power down sequence on my board.
I would like the DM365 to tell the PRTCSS to initiate a power down sequence, the PRTCSS would then need to disable all of the board's supplies in the correct order (as we are using individual regulators/switchers as opposed to a monolithic chip). Is this even possible? It appears that the DM365 must write/read from the PRTCIF which then controls the PRTCSS, but it is not clear to me if the PRTCSS can run entirely on its own.
Thanks for the help!
Rick