Hi,
I have custom design board with C6713B. I am using CCS 3.3 with a 510 Emulator.
I tried executing the example programs but I get the error during the loading of the program on to the memory. (FILE --> LOAD PROGRAM)
I understand that I need to edit the .CMD file or the .GEL file. I have the following query, kindly do provide the pointers to me....
1. Which is better editing .CMD file or the .GEL file ? (My understanding is that I need to use either .CMD file or .GEL file and not both together. Am I correct here ?)
2. Where can I get tutorial on how to create a new .CMD or .GEL file ? (I searched for the tutorial but was not able to find !!)
Kindly do provide me wiht pointers (to links or discussions....etc)
Any help will be appreciated.
Thank you in advance.
Regards
Stevean