hello everyone
I have some question about PCI boot mode on C6455 dsp core.
1. how to download a boot image from PC application ( windows) to DSP board by PCI interface.
-> I 'll write directly a *.bin file that maked by DSP Boot Assist Tool to L2SDRAM(0x0080 0000) to use PC application. is it right method ?
2. how to access the L2SDRAM address
-> I know that the PC application can acess the DSP memory areas by PCIBARx(PCI base address), but PCI auto-initialization is set only Vendor ID, class code, subsys vendor ID, Interrupt pin . how can I set the PCI Windows Config ( PCIBARx, PCIBARxMSK, PCIBARxTRL) registers?
thank you
dhkim