This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEVM572X: How to use DSP in front of GStreamer

Part Number: TMDSEVM572X

(Gstreamer1.0 v1.8/ Linux 4.4)

Hi,

I want to do an application who apply video transformation on a couple of video and audio input with the capability of DSP before doing a streaming of selected audio/video (only one).

I want to now if there is a doc. or software example for my issue :

How to use C66x DSP features to capture (for example) two videos FROM Video Inputs Ports VIP1 VIP2 and two audio FROM AudioIn Left=Audio1 Right=Audio2

And then in the "IVA(?)  Video Acceleration" : How to select the video source in Gstreamer from the DSP video output to use it in a pipeline ?


Thank You