Part Number: DM3730
Tool/software: Linux
Hello,
I am using EVB for dm3730 and can boot from SD and NAND without issues, but I have problems booting from serial.
The sys_boot is configured as following:
| SYS_BOOT_0 | 1 |
| SYS_BOOT_1 | 1 |
| SYS_BOOT_2 | 1 |
| SYS_BOOT_3 | 1 |
| SYS_BOOT_4 | 0 |
| SYS_BOOT_5 | Boot Select |
| SYS_BOOT_6 | 1 |
According to TRM:
- when sys_boot[5] = 0 the boot order is:
0b01111: NAND USB UART3 MMC1
- when sys_boot[5] = 1 the boot order is:
0b01111: USB UART3 MMC1 NAND
I have fully erased nand, removed SD, and try to boot with boot sw (and also tried sw off), but same results: it seems to start xloader for 1 seconds and then it stops.
It is also interesting that sd boot is possible only with sys_boot5=1 (pressing switch) though that according to above boot order, in both options , it also should try SD boot .
Thanks for any idea,
Ran