Part Number: 66AK2G02
Table 4-29 requires a pulldown on ball L5 (TDI) if unused. However according to table 4-1, this ball has a pullup during reset. Won't the pullup and the pulldown conflict? Shouldn't it have a pullup like L3 and K4?
If the pulldown is required, what value is recommended to avoid conflict?
I am assuming that this ball counts as "unused" because though the net is brought to a JTAG header, the JTAG pod is not normally plugged in. Thus it is normally connected to a trace and connector with nothing driving it. Inferring from a note later in section 4.5, this could result in a high current state which could damage the IO cell.