Hello!
We are capturing digital video with DM6435. We have checked that this video is correct (as we are passing it from another device). First of all, we pass it through the resizer to make it smaller. The original incoming video has a size of 720x576 pixels, although we only use part of it (whose size ranges always below VGA). I'm saying this to make it clear that we are not trying to manage huge video frames.
So far, so good. We are checking different sizes for the resizer's output video and we have seen some problems when the image shows any kind of moving object (it doesn't matter its size). At certain sizes (when rising above QVGA) we have the stripe effect that can be seen in the next image around the moving hand:

We have checked that the stripes can be seen before the resizer, so it doesn't look like a resizing matter at all.
Right now we are using the following versions:
· DVSDK 1.01.00.15
· PSP 1.00.02.00
Could it be possible that the stripes are caused because of using old driver versions? Does anyone know? Might it be solved by updating the software?
Thanks a lot in advance!