Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
Dear Sir,
My Application is running on TMS320C6670, Application need Ethernet communication between DSP Board and Linux PC for sending the DATA,
We are running socket server program in Linux PC with static IP configuration and client program is running in DSP board, I am using NDK client example code form “C:\ti\mcsdk_2_01_01_04\examples\ndk\client\evmc6670l”. We are running the code with static IP Address following console output soon below.
I am not able to transmit the data between DSP and Linux machine, please provide what are the modifications required in NDK client program, please provide the solutions.
I am eagerly waiting for reply.
[C66xx_0] PA successfully initialized
[C66xx_0]
[C66xx_0] TCP/IP Stack Example Client
[C66xx_0] PASS successfully initialized
[C66xx_0] Ethernet subsystem successfully initialized
[C66xx_0] Ethernet eventId : 48 and vectId (Interrupt) : 7
[C66xx_0] Registration of the EMAC Successful, waiting for link up ..
[C66xx_0] Network Added: If-1:192.168.1.10
[C66xx_0] Raw Eth Rx Task has been started
[C66xx_0] Service Status: Telnet : Enabled : : 000
[C66xx_0] Service Status: HTTP : Enabled : : 000
[C66xx_0] Raw Eth Task Started ...
[C66xx_0] Raw Eth Task Ended .
Thanks & regards,
Anil Kumar