Other Parts Discussed in Thread: OMAP-L137
CPU: OMAPL137(OMAPL137_v2)
Bootloader : D800K003
Periphral : 100MHz SDRAM, W25X32
BootUtils package version: 2.12
HexAIS_OMAP-L137 version : 1.21.3814.18031
HexAIS_OMAP-L137's ini file:
<ini file start>
[General]
BootMode=SPIMASTER
AddrWidth=24
crcCheckType=SECTION_CRC
[PLLCONFIG]
PLLCFG0 = 0x18010202
PLLCFG1 = 0x00050800
[PERIPHCLKCFG]
PERIPHCLKCFG=0x0000000E
[EMIF3sdram]
SDCR = 0x00018421
SDTIMR = 0x109112A08
SDTIMR2 = 0x70090005
SDRCR = 0x000003FA
<ini file end>
==================================================
I'v develop my project 6 months.My program all run in SDRAM. After OMAPl137 update to V2, I meet two questions.
Q1: sfh_OMAP-L137 halt at "Waiting for SFT on the OMAP-L137..."
cmd: sfh_OMAP-L137.exe -targetType OMAPL137_v2 -flashType SPI_MEM -erase
Q2: After many tests, I downloaded my ais file to spi flash by using spiflash_writer_ccsv3.out.But it cannot startup normally.
AIS file download steps
step1: connect OMAPL137 arm core
step2: download spiflash_writer_ccsv3.out
step3: run,input "dspais", and then input my ais file path.
step4: Wait to finish, and turn the board to spi0 bootmode.
After pown on reboot, OMAPL137 startup abnormally.But When I connect it using CCS,and do "CPU Reset" and "Restart", it works fine.So the program in spi0 flash has been moved in SDRAM.
I also used UartHost and uart tool to load program . It still can not run until CPU reset and restart.
I guess the command "Jump & Close" operate failed, but didn't find out the reason now.