Part Number: AM5728
I can capture the video successfully, but the video offset to right and down.
I used discrete sync.
How can i fix this problem? How to set the Horizontal and the Vertical offsets in the RDK?
RDK version: ti-processor-sdk-linux-am57xx-evm-03.03.00.04
capture chip:adv7612,HDMI in,dual 8BIT out
resolution: 800x600@60
test code: Based on dual-camera-demo-1.0, remove QT dependence.
my dts clips:
&i2c1 {
status = "okay";
clock-frequency = <400000>;
.......
adv7612:adv7612@4c {
compatible = "adi,adv7612";
reg = <0x4c>;
default-input = <0>;
port {
cam: endpoint {
remote-endpoint = <&vin3a>;
hsync-active = <1>;
vsync-active = <1>;
pclk-sample = <0>;
bus-width = <8>;
};
};
};
};
&vip2 {
status = "okay";
};
&vin3a {
status = "okay";
endpoint {
slave-mode;
remote-endpoint = <&cam>;
};
};
Best Regards!
Jia