This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVP 7002 vs. TVP 70025I

Other Parts Discussed in Thread: TVP7002

·        What is the advantage in using TVP-70025I over using the TVP-7002?  It seems to me that the TVP-7002 has all the features as the other device; it can handle higher data rate 165 MHz PCLK; and it cost less. Over all the TVP-7002 seems to be a better choice unless it has much more power consumption than the TVP-70025I -- which is the information I could not find in the datasheet.

Regards,
Sy