Other Parts Discussed in Thread: TMS320DM6467
We are working on our senior design project at school that centers around TMS320DM6467. We are having a hard time getting DDR2 memory chips for this processor becuase most suppliers are requesting that we order large quanties which of course we cannot afford nor do we need.
My question is does the memory interface on TMS320DM6467 require a minimum amount of pins to be connected to the memory chip? The reason for asking this is that most 1.8V 3ns DDR2-667 we are coming across have either 84 or 60 pins. It's looking like we might be able to get the 60-pin (BGA) from Micron (part # MT47H128M8HQ-3 IT:E), but I am a little concerned about the lesser number of pins on the chip especially when compared to the memory chip that was used on the evaluation board which had 92-pins.
Second question, is there a memory density (size) limitation on with TMS320DM6467? We are thinking of using the 2Gb modules instead of the 1Gb memory density used on the evaluation board. Will this be a problem?
Thanks.