This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCI6638K2K: Component Height Clarification

Part Number: TCI6638K2K

Hello,

My customer was recently taking a look at the mechanical drawings on pages 330 and 331 of the TCI6638K2K's datasheet and uncovered some possible inconsistencies that we were wondering if you could clarify?

On page 330, the image below shows a measurement showing max and min heights as 3.75mm and 3.39mm respectively--

While on page 330 we see it stated not only at the topof the page but also in the diagram below that max height is 3.62mm?--

Would you be able to help us understand what the actual max, min and typ. measurements are for height of this device?

Appreciate your time and direction!

-Amanda