Hello,
In order to control two three phase motors in our system, PRU-ICSS needs to process Sigma Delta Decimation Filtering and perform four current sensing. (I1u, I1v, I2u and I2v)
The SDDF processing channel is described in the following documents.
"Three channels are used for current (5, 6, & 7), channel '1' is used for voltage (which is disabled by default)."
C:\ti\PRU-ICSS-Industrial_Drives_01.00.00.00\interfaces\sddf\doc\SigmaDelta_am437x_design.pdf
Can PRU-ICSS perform four current sensing simply by setting arguments to the driver API without customizing the firmware or the driver source code?
Regards,
Kazu