I used two TMS320C6678 DSP in my system. And connect each other used the Hyperlink and connect to Xilinx FPGA(A7) used the SRIO. Hyperlink Speed: 12.5Gbps; SRIO Speed: 3.125Gbps.
In order to meet the performance, I used the Hyperlynx and IBIS model to simulate the hyperlink and SRIO.
But there is not IBIS model in hyperlink pins and SRIO pins.
e.g:
so can you help me to select the high speed IBIS mode for hyperlink/SRIO/SGMII/PCIe simulation?
If you have the newest IBIS model or IBIS-AMI model. Can you provide them to me?