This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM643x PSP_1.10.03 vpbe sample project - CCS build error due to illegal package pathname syntax

Other Parts Discussed in Thread: CCSTUDIO

Hi BIOS/PSP Champs,

I tried to build the DM6437 VPBE example delivered with the DM643x PSP drivers  (Version 1.10.03) without any manual modifications. However, I experienced following error:

-------------------  dm6437_evm_vpbe_st_sample.pjt - Debug  -------------------
[dm6437_evm_vpbe_st_sample.cfg]
"C:\Program Files\Texas Instruments\xdctools_3_16_02_32\xs.exe" xdc.tools.configuro.ccs  --xdcpathsfile="xdcpaths.dat" -tti.targets.C64P -pti.platforms.evmDM6437 -rdebug --tcf -Dconfig.importPath=".;../;C:/Program Files/Texas Instruments/pspdrivers_1_10_03/packages/ti/sdo/pspdrivers/system/dm6437/bios/evmDM6437/video/sample/build/vpbe/..;" -w -c "C:/Program Files/Texas Instruments/C6000 Code Generation Tools 6.1.14" --xp "C:/CCStudio_v3.3/bios_5_33_06/packages" -o "xdcconfig" dm6437_evm_vpbe_st_sample.cfg
js: "C:/Program Files/Texas Instruments/xdctools_3_16_02_32/include/utils.tci", line 727: An entry on the package path has illegal pathname syntax: " C:\CCStudio_v3.3\bios_5_33_06\packages" Full package path is C:\Program Files\Texas Instruments\pspdrivers_1_10_03\packages; C:\CCStudio_v3.3\bios_5_33_06\packages; C:\Program Files\Texas Instruments\xdctools_3_16_02_32\packages; C:\Program Files\Texas Instruments\edma3_lld_01_10_00_01\packages;C:\Program Files\Texas Instruments\xdctools_3_16_02_32/packages;.;
Build Complete,
 
1 Errors, 0 Warnings, 0 Remarks.


For me it seems that the last pathname (yellow shaded) with the '/' instead of '\' may cause the illegal path syntax error. Would you agree with my assumption? In which file or at what location can I correct the wrong syntax?

 

To give you a better picture here is my complete setup:

  • CCS Version 3.3.82.13 (CCSv4 Version 4.1.2 also installed)
  • C6000 CGT Version 6.1.14
  • PSP Version 1.10.03
  • DSP/BIOS Version 5.33.06
  • EDMA3 LLD Version 1.10.00.01
  • XDCtools Version 3.16.02.32 (That's the only version that I can select in CCS3.3. Older Versions are available but Component Manager does not show them)
  • Environment Variables
    • BIOS_INSTALL_DIR=C:\CCStudio_v3.3\bios_5_33_06
    • XDCPATH=C:\Program Files\Texas Instruments\pspdrivers_1_10_03\packages; C:\CCStudio_v3.3\bios_5_33_06\packages;
      C:\Program Files\Texas Instruments\xdctools_3_16_02_32\packages; C:\Program Files\Texas Instruments\edma3_lld_01_10_00_01\packages
    • XDCROOT=C:\Program Files\Texas Instruments\xdctools_3_16_02_32
  • Updated the file "psp_xdcpaths_common.dat" with the correct pathnames

Thank you very much in advance for your guidance and best regards,

Peter.