This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/LINUXSDK-OMAPL138: OMAPL138 with wifi usb adapter

Part Number: LINUXSDK-OMAPL138


Tool/software: Linux

Hi,

I am working with the OMAP L 138 and want to connect a wifi usb adapter from EDIMAX (EW-7811Un)

this wifi usb adapter works with the raspberry pi very well, there is no driver needed.

The OMAP L 138 has a Linux OS with a 3.3 Kernel, where it should also run very well.

The problem is that the OMAP OS has not the make package to install drivers.

Did anybody make experience with wifi usb adapter s  for the OMAP L 138?