This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVMFlash - not connecting to target



I'm trying to reflash my OMAP EVM MAIN BOARD REV G, but am having trouble with the EVMFlash3530_v2.0 utility.  After I click Download and power on the board, I only get an error message titled "EVMFlash" that states "Failed to connect to target".  I recently tried to put Android on the board before deciding to go with Windows CE, so I'm not sure if I messed something up in the environment variables that is causing this to fail.  I just want to put the original NAND flash back on so I can start from scratch.

Also, I see a place on the EVMFlash tool for DEBUG, but I'm not sure how to look at debug output.  Maybe since it's not connecting there is no debug file yet?  Any help would be greatly appreciated!!