Part Number: TMS320C6742
Hi Support,
My customer is developing the firmware on TMS320C6742 and encounter an issue.
He is using emulator XDS200 and CCS 6.2.0.00050 to test his firmware on the custom board.
When stepping to debug his code after board power up, the firmware was running well.
But if run it continuously after board power up, it will stuck at address 0x713d4e and report the error No source available for "0x713d4e".
But 0x713d4e is in the address of DSP L2 ROM, which stores the factory boot loader.
Any idea why it could happen?
Thanks.