Tool/software: TI-RTOS
I am working on PRU-ICSS-EtherCAT_Slave_01.00.02.01 industrial SW package and able to build the ethercat_slave_full_AM335x_arm project.
But this project is not generating "_ti.bin" file anymore. It generates ethercat_slave_full_AM335x_arm.out and ethercat_slave_full_AM335x_arm.bin. I am able to download the ".out" file using a debugger and run the application. But when I am loading the ".bin" file then it is not working.
Do we need to generate _ti.bin file now or it is not required anymore?
regards
Mohit