Hi,
i'm using c5515 eZdsp in order to acquire a dsbsc modulated signal. My goal is to demodulate the signal.
The signal acquisition is made using ping pong buffer (only input left channel), taken from C5515_Audio_Filter demo code.
My algo is: FFT, frequency ***, IFFT.
The demodulation succeeds, but in the transition from an input buffer from another i have a bad spike that distances my output signal:
in main.c:
while(1)
if(CurrentRxL_DMAChannel == 2)
{
buff_copy(RcvL1,BufferL1,XMIT_BUFF_SIZE);
dsb_sc_demod(BufferL1);
buff_copy(BufferL1,&FilterOutL1[0], XMIT_BUFF_SIZE);
}
else if(CurrentRxL_DMAChannel == 1)
{
buff_copy(RcvL2,BufferL2,XMIT_BUFF_SIZE);
dsb_sc_demod(BufferL2);
buff_copy(BufferL2,&FilterOutL2[0], XMIT_BUFF_SIZE);
}
}
dsb_sc_demod():
void dsb_sc_demod(Int16 *input){
Uint8 i;
Uint8 idx;
const Uint8 iMAX = FFT_LENGTH/2;
if(freq == FREQ_32)
idx = CARRIER_32_IDX;
else
idx = CARRIER_42_IDX;
do_fft(input, realL, imagL, 1);
for(i = 0 ; i < iMAX; i++){
*(realL + i) = *(realL + i + idx);
*(imagL + i) = *(imagL + i + idx);
}
for (i = 1; i < FFT_LENGTH/2; i++) {
*(realL + FFT_LENGTH - i) = *(realL + i );
*(imagL + FFT_LENGTH - i) = -*(imagL + i );
}
do_ifft(realL, imagL, input, 0);
}
In the following image you will see a spike:
Do you have any suggestion to avoid this?
Thanks
Paolo