Hi,
I have a board which the C6713b DSP processor used to boot from a flash memory. Now, it won't. I have verified that the HD[4,3] are set to 10 to enable loading from flash before and after reset. Is there anything else that could prevent the board from starting up? Is there a good way to determine if something is wrong with the processor. It still runs from the emulator with the program, but it wont boot from the flash.
Thanks
Noe.