This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDXIDK5718: IDK fails to start

Part Number: TMDXIDK5718

   I download am57xx-evm-linux-rt-03.02.00.05 , and I use  Win32DiskImager to download the image into the SD card according the "Windows SD Card Creation Wiki". 

Then I insert the SD into the IDK and power on the IDK. there no outport from the serial port. It seems  the software is blocking.I wonder if this IDK is failure.