This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux: linux base low cost processor

Other Parts Discussed in Thread: AM3358

Tool/software: Linux

 I want to develop Linux base low cost platform for my project i was thinking of Linux instead of ucLinux.

can anyone suggest me the best processor/uc for which Linux image will be easily available .

My requirement is small LCD ~3", SPI,I2C,USB2.0,Fifi speed will be at approximately  450MHz .

And all components must not be BGA package.

If any open source design is available for reference please provide me link or any material.