Part Number: DRA744
Tool/software: Linux
Hi,
I have booting the DRA744 on uboot process.
Some time will stop the boot process that I have check the power sequence and power of PMIC is ok.
The related log as below,
Could any one please tell me how can I debug this issue?
Thank you.
U-Boot SPL 2014.07 (May 09 2017 - 17:39:04)
DRA752-GP ES1.1
IODELAY: Isolation of Device IOs failed
ti_i2c_eeprom_init failed 1
===lisa_map_dra7_1536MB===
===EMIF-(1) Interface Setting===
===Ram Size = 0x0 ===
Use emif1_ddr3_532_mhz_1cs
===EMIF-(2) Interface Setting===
===Ram Size = 0x0 === SDRAM: identified size not same as expected size identified: 4 expected: 40000000