This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PSP for Zoom OMAP L138 eXperimenter Kit

Other Parts Discussed in Thread: OMAP-L138

Hi,

I got Zoom OMAP L138 eXperimenter Kit from Logic PD. I have installed all the software and setup the development environment as per the below links.

http://processors.wiki.ti.com/index.php?title=Getting_Started_Guide_for_OMAP-L138

http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/omap_l138/1_00/latest/index_FDS.html

 

In my installation directory, "OMAP-L138_arm_1_00_00_11", I have the below folders:

(1) DaVinci-PSP-SDK-03.20.00.11

(2) pspdrivers_01_30_01

 

Initially, I got confused why there are 2 PSP folders. After I read some documentation, it seems to me "DaVinci-PSP-SDK-03.20.00.11" is PSP for Linux at the ARM side, whereas "pspdrivers_01_30_01" is PSP for DSPBIOS at the DSP side.

 

Is this correct ?

 

rgds,

kc Wong