Part Number: TMS320VC5509A
-
What CPU_XXX bugs are still in the 5509a and 5510a silicon dies?
-
Can we get more info on CPU_120 to CPU_127?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320VC5509A
What CPU_XXX bugs are still in the 5509a and 5510a silicon dies?
Can we get more info on CPU_120 to CPU_127?
Hi David Johansson86 (4455186)
I have tried to dig through various bug tracking systems and archives, and unfortunately there are no known owners for these devices from a design/development standpoint , so the data I have pulled is based on what I can cobble together based on what I see in the archives
To the best of my knowledge here following is the story on the addition CPU bugs for the devices you are interested in
| 5507 | 5509A | 5510a | |
| CPU Revision | v2.2 | v2.2 | v2.11 |
| CPU_120 | |||
| CPU_121 | |||
| CPU_122 | x | x | |
| CPU_123 | x | x | x |
| CPU_124 | |||
| CPU_125 | x | x | x |
| CPU_126 | x | x | x |
| CPU_127 | x | x | x |
| CPU_128 | x | x | x |
x implies bug is present/applicable.
I will be out next week, and once I am back I will try to see if I can verify this further with someone with additional background on this.
Any questions on CCS/compiler workarounds etc for these devices will likely need to be addressed by folks in the CCS forum team.
Regards
Mukul
Hi Mukul and David,
Is there some documentation on what cpu_124 to cpu_128 mean? I have checked the following sources with no luck:
CCS release notes:
'readme 3.2.2.txt'
'readme 3.2.3.txt'
'readme 3.3.3.txt'
'readme 3.3.4.txt'
'readme 3.3.5.txt'
'readme 3.3.6.txt'
spru652g.pdf
sprz006e.pdf
sprz008o.pdf
sprz200f.pdf
sprz217c.pdf
And also

Best regards, and thanks in advance
Hi Santiago
This is somewhat non trivial and I will need to discuss internally. It will also take us several weeks in my opinion as the bug reports are in an internal bug repo and not in document format that can be shared.
I will keep you posted if there is anything I can offer to help on this. As you can imagine this is almost 15+ year old data.
On a positive note, it appears that CPU_125 and 126 will not be relevant to customers.
So the list of ones that maybe relevant for you is smaller.
Regards
Mukul