This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2EVM5777: single channel use case failed to run

Part Number: TDA2EVM5777

Hi all,

I was trying to learn use cases for TDA2X vision SDK, and I successfully bring up those surround view use cases for multi channels.

But I failed to run the single channel use cases and it gave me the following errors.

I followed the user guide for bringing up multi channel use cases and succeeded, but I don't find any specific use guide for single channel. So, I assume they should be the same.

Can anyone help to check this issue? And what kind of modification I need to bring up the single channel use case.

Thanks.

Yunpeng

  • Hi Yunpeng,

    Typically the 1CH VIP Capture use cases work with the OmniVision image header boards, LI single imager via flex cable and Aptina image header boards that are interfaced with the appropriate connectors on the Vision Apps board. Also please check your settings 's' to configure your setup before you select and start a use case.

  • Hi Ewald,

    Thanks for your reply. Currently, I'm using the SAT0089 board to connect the TDA2EVM board because I want to use the surround view use case. Also, I'm working on the Windows SDK. I don't have the Aptina or Omvision image header boards available at hand. So, is it possible to bring up the OpenCV use case with my current hardware components? I think there's some configuration to change for the SAT0089 board in the SDK.

    Here's the overview of my system:

    Thanks.

    Yunpeng