Part Number: AM3354
Hi,
We have designed a custom board using AM3354,
We designed the board considering MMC0 be used as a booting media, but as there is a restriction for boot device should be less than 4GB.
There is also nand on the board and made configuration to boot from nand and we are able to boot from NAND
Question :
1. Can we run the application from MMC (4GB eMMC connected to MMC0) when Linux is booted fron NAND(Connected to GPMC) ?
2. Is there any restriction for memory size for NAND boot (8bit or 16 bit) ?
Regards
Sujay A